MMEMory:STORe:CONVerter <string>,<char>

(Write-Only) Store a frequency converter corrections file (*.csv) file to a specified device.

Note: Unless otherwise specified, on the FieldFox, *.csv files are initially stored and recalled by default from the "[INTERNAL]:\Converter" folder.

To load a frequency converter corrections file, use MMEMory:LOAD:CONVerter.

See ALL MMEM commands.

Relevant Modes

EMI, SA

Parameters

 

<string>

For *.csv files, provide filename of the *.csv file WITHOUT an extension.

<char>

Memory device where the frequency converter corrections file is stored. Choose from the following:

  • INTernal - internal storage device

  • USB - first USB device

  • SD - SD storage card

Examples

MMEM:STOR:CONV "MyDUT",INT 'Stores a corrections file "MyDUT" to INTernal FieldFox memory.

Query Syntax

Not Applicable

Default

Not Applicable


Last Modified:

04no2022

Added EMI mode (12.3x)

20apr2020

New command A12.00