MMEMory:LOAD:CONVerter  <string>,<char>

(Write-only) Loads a frequency converter corrections file (*csv) from specified device (INT | USB | SD).

Note:

  • This command is not needed, when Auto loading is set using SYST:HEAD:CORR:ASET.

  • Unless otherwise specified, on the FieldFox, *.csv files are initially stored and recalled by default from the "[INTERNAL]:\Converter" folder.

To store a frequency converter corrections file, use MMEMory:STORe:CONVerter.

See ALL MMEM commands.

Relevant Modes

EMI, SA

Parameters

 

<string>

For *.csv files, provide filename of the *.csv file WITHOUT an extension.

<char>

Load a frequency converter corrections file from user data. Choose from the following:

  • INTernal - internal storage device

  • USB - first USB device

  • SD - SD storage card

Examples

MMEM:LOAD:CONV "MyCONV_File",INT 'loads a file "MyCONV_File" from INTernal memory.

Query Syntax

Not Applicable

Default

Not Applicable


Last Modified:

04no2022

Added EMI mode (12.3x)

20apr2020

A12.00 New command