|
(Read-Write) Set and query the RTSA and SA modes burst alignment (InstAlign) state. |
|
|
Relevant Modes |
All models with InstAlign capability (All EXCEPT N9912A). |
|
Parameters |
|
|
<char> |
InstAlign state. Choose from: AUTO - The alignment process is performed every 300 seconds or when the temperature has changed about 1 degree. It occurs only at the beginning of a sweep and takes about 0.5 seconds to complete. HOLD - The alignment process is stopped, but the last alignment values are applied to subsequent sweeps. OFF - The alignment process is NOT performed. Only factory correction values are used. |
|
Examples |
ALIG:BURS HOLD |
|
Query Syntax |
[:SENSe]:ALIGnment:BURSt[:STATe]? |
|
Return Type |
Character |
|
Default |
AUTO |
Last Modified:
|
04no2022 |
Added EMI mode (12.3x) |
|
22oct2017 |
New command & new IQA mode (A.10.15) |