|
(Write only) Initiates an audio capture, which is saved as an audio file when the capture is complete (the file name, file type and storage device used are determined by the Audio Capture File Settings). This command is overlapped. This means that it will execute and, while the FieldFox performs an audio capture, it will also accept new commands. Follow this command with *OPC? to cause the FieldFox to wait before accepting subsequent commands. See also, AUD:CAPT:STOP and MMEM:LOAD:AUD. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
|
|
|
Examples |
AUD:CAPT:STAR */Initiates an audio capture |
|
Query Syntax |
n/a |
|
Return Type |
n/a |
|
Default |
n/a |
Last Modified:
|
01june2021 |
New command (A.12.3x) |