[:SENSe]:BURSt:ALIGnment[:STATe]

This command has been replaced by [:SENSe]:ALIGnment:BURSt[:STATe]. Learn about superseded commands.

(Read-Write) Set and query the RTSA and SA modes burst alignment (InstAlign) state.

Relevant Modes

IQA, SA, CPM, RTSA

All models with InstAlign capability (All EXCEPT N9912A).

Parameters

 

<char>

InstAlign state. Choose from:

AUTO - The alignment process is performed every 300 seconds or when the temperature has changed about 1 degree. It occurs only at the beginning of a sweep and takes about 0.5 seconds to complete.

HOLD - The alignment process is stopped, but the last alignment values are applied to subsequent sweeps.

OFF - The alignment process is NOT performed. Only factory correction values are used.

Examples

BURS:ALIG HOLD

Query Syntax

[:SENSe]:BURSt:ALIGnment[:STATe]?

Return Type

Character

Default

AUTO


Last Modified:

22nov2017

Updated as a superseded note & added IQA for backwards compatibility.

20-sep-2016

Added RTSA mode (A.09.50)

1-Apr-2014

Added CPM

28-Mar-2013

Changed time from 30 to 300 secs

17-Jul-2012

New command (6.00)