|
(Write-Only) Measures the internal (Quick Cal) standard for the specified port. Prompt to leave the port OPEN for this step. Use [:SENSe]:CORRection:COLLect:METHod:QCALibrate:CALibrate for both 1-port and 2-port QuickCal. Use [:SENSe]:CORRection:COLLect[:ACQuire]:LOAD for the optional LOAD measurement. This command is overlapped. This means that it will execute and, while the FieldFox measures the cal standard, it will also accept new commands. Follow this command with *OPC? to cause the FieldFox to wait before accepting subsequent commands. |
|
|
Relevant Modes |
CAT, NA To Cal in VVM mode, perform a Cal in CAT or NA mode, then switch to VVM mode. |
|
Parameters |
|
|
<num> |
Port number to calibrate. N9912A - Choose 1 (RF OUT) All others - Choose 1 or 2 |
|
Examples |
CORR:COLL:INT 1 |
|
Query Syntax |
Not Applicable |
|
Default |
Not Applicable |
Last Modified:
|
18-Oct-2012 |
Modified for new models |