[:SENSe]:CORRection:COLLect:METHod:QCALibrate:CALibrate <p1>[,p2]

(Write-Only) Sets the Cal Method to 1-port or 2-port QuickCal.

Note: QuickCal commands do not apply to N995x/6xA or B model FieldFoxes.

For 1-port QuickCal:

For 2-port QuickCal with Insertable connectors, performs QSOLT.

For 2-port QuickCal with Non-Insertable connectors, performs SOLR.

  • Prompt for INT Stds on <p1> and <p2>, then optional LOAD on <p1> and <p2>, then ANY THRU.

 

Learn more about FieldFox Cal Methods using SCPI.

Relevant Modes

CAT, NA

To Cal in VVM mode, perform a Cal in CAT or NA mode, then switch to VVM mode.

Parameters

 

<p1>

First port to calibrate.

  • For N9912A, choose 1.

  • For all other models, choose 1 or 2.

[p2]

For all models with Full S-parameter option, second port to calibrate.

Choose 1 or 2  (alternate to <p1>).

Examples

CORR:COLL:METH:QCAL:CAL 1,2

See Cal examples

Query Syntax

Not Applicable

Default

Not Applicable


Last Modified:

02apr2019

Added B model content

18-Oct-2012

Added new models