|
(Write-Only) Measures the THRU calibration standard that is connected between the specified ports. This can be used in any of the following Cal Methods:
This command is overlapped. This means that it will execute and, while the FieldFox measures the cal standard, it will also accept new commands. Follow this command with *OPC? to cause the FieldFox to wait before accepting subsequent commands. |
|
|
Relevant Modes |
CAT, NA To Cal in VVM mode, perform a Cal in CAT or NA mode, then switch to VVM mode. |
|
Parameters |
|
|
<p1>,<p2> |
Port numbers to which the THRU standard is connected. Choose 1,2 |
|
Examples |
CORR:COLL:THRU 1,2 |
|
Query Syntax |
Not Applicable |
|
Default |
Not Applicable |
Last Modified:
|
18-Oct-2012 |
Reviewed for new models |