[:SENSe]:CORRection:ENR:MODe <char>

(Read-Write) Set and query the ENR mode preference. If two noise sources are connected (USB Smart Noise Source and normal), this parameter will decide which one is used for measurement and calibration.

NOTE:

See also [:SENSe]:CORRection:ENR:SPOT:ENR, [:SENSe]:CORRection:ENR:UNCertainty, [:SENSe]:CORRection:ENR:ONGamma, [:SENSe]:CORRection:ENR:OFFGamma, [:SENSe]:CORRection:ENR:COVerage, [:SENSe]:CORRection:ENR:SPECify, [:SENSe]:CORRection:ENR:DISTribution, CORR:ENR:NOIS:STAT, CORR:ENR:NOIS:CONN, CORR:ENR:AUTO, and CORR:TCOL.

Relevant Modes

 NF

Parameters

 

<character>

ENR mode. Choose from:

SMARt -  When set to SMARt mode, the Noise Source Control menu is enabled and accessible.  

To learn more about Smart Noise Sources, refer to https://www.keysight.com/us/en/products/noise-figure-analyzers-noise-sources/noise-sources.html.

SPOT -  You can enter ENR data for the noise source you are using as a single spot value.
The single spot value is used either for measurements at a single frequency, or for measurements across a range of frequencies that is narrow enough such that the ENR value does not change significantly across that range.

TABLe - You can enter ENR data for the noise source you are using as a table of values. The values held in the table can be used for measurements at a range of frequencies as well as at a fixed frequency. But, other integration values cannot be set.

Examples

CORR:ENR:MOD SPOT */Turns on the Smart source (default)

CORR:ENR:MOD TABL */Sets ENR data source to TABL

Query Syntax

CORRection:ENR:MODe?

Return Type

Character

Default

TAB


Last Modified:

06sept2022

Added: NF mode updates for smart source feature (A.12.5x)

01june2018

Added NF mode Opt. 356 (10.3)