[SENSe]:CORRection:LOSS:AFTer:TEMPerature <double>

(Read-Write) Set and query the loss correction values after the DUT (DUT In). Returns a the temperature correction in double numerical format.

See also CORRection:LOSS:AFTer[:VALue] and CORRection:LOSS:AFTer:ENABLed.

Relevant Modes

NF

Parameters

 

<double numbers>

Enter values in Centigrade, Fahrenheit, or Kelvin. All values converted to Kelvin.

Examples

:CORR:LOSS:AFT:TEMP 87.43 (Converts any value entered to Kelvin units.)

Query Syntax

:CORRection:LOSS:AFTer:TEMPerature?

Return Type

double numbers

Default

296.50K


Last Modified:

01-june-2018

Added Opt. 356 NF(10.3)