(Read-Write) Set and query the Preamplifier uncertainty setup values being measured. See also [:SENSe]:CORRection:PAMPLifier:INGamma, [:SENSe]:CORRection:PAMPLifier:OUTGamma, [:SENSe]:CORRection:PAMPLifier:SPEC, [:SENSe]:CORRection:PAMPLifier:DISTribution. See also, MMEMory:LOAD:PAMPLifier and MMEMory:STORe:PAMPLifier. |
|
Relevant Modes |
|
Parameters |
|
<character> |
Preamplifier mode uncertainty settings. Choose from: SPOT- Sets the Preamplifier mode to Spot, where you can customize the ENR values for your device. TABL - Time per point can be set, but other integration SCPIs are not settable. |
Examples |
CORR:PAMPL:MOD SPOT CORR:PAMPL:MOD TABL |
Query Syntax |
CORRection:PAMPL:MODe? |
Return Type |
Character |
Default |
SPOT |
Last Modified:
01june2018 |
Added NF mode Opt. 356 (10.3) |