(Read-Write) Set and query the preamplifier's specified fixed value. This value indicates the nature of the entered value relative to the population of values it represents. Note: Only available when CORR:PAMP:MOD is set to SPOT. See also [:SENSe]:CORRection:AMPLifier:SPOT:INGamma, [:SENSe]:CORRection:PAMPLifier:SPOT:OUTGamma, [:SENSe]:CORRection:PAMPLifier:MODe, [:SENSe]:CORRection:PAMPLifier:SPOT:DISTribution. See also, MMEMory:LOAD:PAMPLifier and MMEMory:STORe:PAMPLifier. |
|
Relevant Modes |
|
Parameters |
|
<character> |
Preamplifier Spot mode's fixed value. Choose from: MAX - Use this if this value represents the largest possible reflection coefficient for the population of devices to which the preamplifier belongs. This is true for "does not exceed" specifications. PCTL95 - Use this if 95% of the population has a lower reflection coefficient than the value entered. This is the case for "2 standard deviation" (2s) type specifications. PCTL80 - Use this if 80% of the population has a lower reflection coefficient than the value entered. MED or MEAN - Use this if this value represents the median / mean reflection coefficient for the population of devices to which the preamplifier belongs. FIX - Use this if the value is a measured value for the preamplifier. |
Examples |
CORR:AMP:SPOT:SPEC PCTL95 CORR:AMP:SPOT:SPEC MED |
Query Syntax |
CORRection:AMP:SPOT:SPEC? |
Return Type |
Character |
Default |
FIX |
Last Modified:
01june2018 |
Added NF mode Opt. 356 (10.3) |