[:SENSe]:POWer[:RF]:ARANge

(Write only) Executes an auto-range, which determines the optimal RF attenuation and preamp settings for the current input signal. If more than one CC is enabled when an auto-range is executed, the range is determined for each CC separately and the final RF attenuation and preamp settings are determined using the maximum range.

Note: Executing an auto-range DOES NOT change any of the display settings (Ref Level, Scale or Ref Pos).

See also, [:SENse]:POWer[:RF]:RLEVel, [:SENSe]:POWer[:RF]:ATTenuation, [:SENSe]:POWer[:RF]:GAIN[:STATe].

Relevant Modes

LTE FDD, 5G TF, 5G NR, 5G NR EVM Conducted

Parameters

 

 

n/a

Examples

POW:ARAN */Executes an auto-range as described above.

Query Syntax

n/a

Return Type

n/a

Default

n/a


Last modified:

01june2022

New command (A.12.5x)