[:SENSe]:POWer[:RF]:GAIN[:STATe] <bool>

(Read-Write) Set and query preamplifier state. Available with Option 235.

See also, [:SENSe]:POWer[:RF]:ARANge.

Relevant Modes

5GTF, 5G NR, 5G NR EVM Conducted, EMI, PAA, PAA, SA, LTE FDD, RTSA, IQA

Parameters

 

<boolean>

Preamp ON | OFF state. Choose from:

O or OFF - (For 5GTF and LTE FDD only OFF is valid) Preamp OFF

1 or ON - (For 5GTF and LTE FDD only ON is valid) Preamp ON

AUTO - (5GTF, LTE FDD, and RTSA Onlyl) When Auto is selected, the preamp setting is coupled to the RF attenuation and to the reference level. When the reference level reaches a certain value, the preamp is turned on and PA is shown to the left of the graticules on the display.

For IQA, see also POW:GAIN:AUTO.

Examples

POW:GAIN 0        '0 and 1 are invalid choices for 5GTF and LTE FDD

POW:GAIN AUTO     '5GTF, LTE FDD, and RTSA Only

Query Syntax

[:SENSe]:POWer[:RF]:GAIN[:STATe]?

Return Type

Boolean

Default

OFF


Last Modified:

31oct2019

Added PAA mode

03dec2018

Added LTE FDD & 5GTF (A.11.0)

22oct2017

Added IQA mode (10.1x)

10-june-2016

Added RTSA mode (9.50)