(Read-Write) Set and query RF attenuation value. Also set POW:ATT:AUTO OFF, [:SENSe]:POWer[:RF]:ARANge. |
|
Relevant Modes |
5GTF, 5G NR, 5G NR EVM Conducted, EMI, PAA, SA, LTE FDD, CPM, RTSA, IQA |
Parameters |
|
<numeric> |
Attenuation value in dB. Choose a number between the minimum and maximum attenuation of the FieldFox. This command will accept MIN and MAX as arguments. The RF Attenuation value is never automatically lowered below 5 dB. CPM mode only accepts two values: 10 dB or 30 dB |
Examples |
POW:ATT 30 |
Query Syntax |
:POWer:ATTenuation? |
Return Type |
Numeric |
Default |
10 |
Last Modified:
31oct2019 |
Added PAA mode |
03dec2018 |
Added LTE FDD & 5GTF (A.11.0) |
22oct2017 |
Added IQA mode (10.1x) |
10-june-2016 |
Added RTSA mode (9.50) |
1-April-2014 |
Added CPM |