|
(Write only) Executes an auto-range, which determines the optimal RF attenuation and preamp settings for the current input signal. If more than one CC is enabled when an auto-range is executed, the range is determined for each CC separately and the final RF attenuation and preamp settings are determined using the maximum range. Note: Executing an auto-range DOES NOT change any of the display settings (Ref Level, Scale or Ref Pos). See also, [:SENse]:POWer[:RF]:RLEVel, [:SENSe]:POWer[:RF]:ATTenuation, [:SENSe]:POWer[:RF]:GAIN[:STATe]. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
n/a |
|
|
Examples |
POW:ARAN:RUN */Executes an auto-range as described above. |
|
Query Syntax |
n/a |
|
Return Type |
n/a |
|
Default |
n/a |
Last modified:
|
06june2025 |
Updated the command to add a corresponding node. |
|
01june2022 |
New command (A.12.5x) |