[:SENSe]:POWer[:RF]:EXTGain <num>

(Read-Write) Set and query external gain value. Use to compensate the trace and scale when using an external amp or attenuator. May automatically increase the amount of attenuation.

Relevant Modes

5GTF, 5G NR, 5G NR EVM Conducted, EMI, PAA, SA, LTE FDD, RTSA, IQA

Parameters

 

<numeric>

Amount of gain (positive value) or loss (negative value) in dB.

This command will accept MIN and MAX as arguments.

Minimum: -100 dB

Maximum: 100 dB

Examples

POW:EXTG 10

Query Syntax

[:SENSe]:POWer[:RF]:EXTGain?

Return Type

Numeric

Default

0


Last Modified:

31oct2019

Added PAA mode

03dec2018

Added LTE FDD & 5GTF (A.11.0)

22oct2017

Added IQA mode (10.1x)

10-june-2016

Added RTSA mode (9.50)