TRACe<n>:DATA? <char>

(Read-Only) Returns the current data trace values. If correction is ON, then the returned data is corrected.

Relevant Modes

 EMI, PAA, NF, SA, RTSA, VVM

For CAT mode and NA mode, use CALCulate:DATA:<type> commands.

Parameters

 

<n>

Trace number of data to be returned.

SA Only. Choose from 1 through 4.

NF Only. Chose from 1 through 2.

If unspecified, <n> is set to 1.

<char>

Note: These parameters are NOT allowed for NF, RTSA and SA mode.

Type of data to return.  Choose from:

FDATA - (VVM Only) Data in the current display format.  

SDATA - (VVM Only) Raw (non-formatted) complex data.   

VVM Mode always returns two data points: Mag and Phase.

Examples

TRACE:DATA? FDATA  'VVM mode. Assumes n = 1

TRAC2:DATA?  'NF, SA, & RTSA mode

Return Type

Comma-separated numeric

Default

Not Applicable


Last modified:

04no2022

Added EMI mode (12.3x)

01june2018

Added NF mode Opt. 356 (10.3)

19-sep-2016

Added RTSA to relevant modes (A.09.50).

28-Oct-2011

Added link to format:data