[:SENSe]:SEMask:OASPan <bool>

(Read-Write) Set and query the Frequency control menu (Center and Span) provides an SEM Auto Span control (defaulted to ON) which automatically tracks the necessary span to cover all enabled offset segments. But you can de-couple the span simply by narrowing or widening Span it in order to zoom.

See also [:SENSe]:SEMask:REFChannel:CENTer and [:SENSe]:SEMask:REFChannel:CENTer:AUTO.

Relevant Modes

SA

Parameters

 

<booleon>

Choose from:

OFF (0) - SEM Auto span control  is disabled.

ON (1) - SEM Auto span control is enabled.

Examples

SEM:OASP 0 'disables the SEM Auto span setting.

SEM:OASP ON 'enables SEM Auto span setting.

Query Syntax

SEM:OASP?

Return Type

numeric

Default

1


Last modified:

01dec2019

Added to SA