(Read-Write) Set and query the SEM reference channel center auto status. When enabled, this feature maintains the center frequency exactly at the Carrier Center and the Span matching what is required for the active Offsets. See also [:SENSe]:SEMask:REFChannel:CENTer and [:SENSe]:SEMask:OASPan. |
|
Relevant Modes |
|
Parameters |
|
<booleon> |
Choose from: OFF (0) - SEM reference channel Auto control is disabled. ON (1) - SEM reference channel Auto control is enabled. |
Examples |
SEM:REFC:CENT:AUTO 0 'disables the SEM reference channel Auto setting. SEM:REFC:CENT:AUTO ON 'enables SEM reference channel Auto setting. |
Query Syntax |
SEM:REFC:CENT:AUTO? |
Return Type |
numeric |
Default |
1 |
Last modified:
01dec2019 |
Added to SA |