[:SENSe]:SEMask:REFChannel:BANDwidth[:RESolution]:AUTO <bool>

(Read-Write) Set and query the SEM resolution bandwidth Auto setting.

See also [:SENSe]:SEMask:REFChannel:CENTer and [:SENSe]:SEMask:OASPan.

Relevant Modes

SA

Parameters

 

<booleon>

Choose from:

OFF (0) - SEM resolution bandwidth Auto control is disabled.

ON (1) - SEM resolution bandwidth Auto control is enabled.

Examples

SEM:REFC:BAND:AUTO 0 'disables the SEM resolution bandwidth Auto setting.

SEM:REFC:BAND:AUTO ON 'enables SEM resolution bandwidth Auto setting.

Query Syntax

SEM:REFC:BAND:AUTO?

Return Type

numeric

Default

1


Last modified:

01dec2019

Added to SA