[:SENSe]:SEMask:REFChannel:IBW  <num>

(Read-Write) Set and query a SEM frequency range integrated bandwidth value where the total power will be summed.

See also [:SENSe]:SEMask:REFChannel:SPAN,  [:SENSe]:SEMask:REFChannel[:RESolution], and [:SENSe]:SEMask:REFChannel[:RESolution]:AUTO.

Relevant Modes

SA

Parameters

 

<numeric>

Choose from:

Dynamic: Changes with models and options.

This command accepts MINimum and MAXimum commands.

Examples

SEM:REFC:IBW 3.84 MHz 'Sets the SEM integrated bandwidth to 3.84 MHz.

SEM:REFC:IBW MIN 'Sets the SEM integrated BW to a minimum value for the model/options.

Query Syntax

SEM:REFC:IBW?

Return Type

numeric

Default

Dynamic: model/option dependent


Last Modified:

01dec2019

New command