Note: This command was previously named [:SENSe]:ISOurce:NORMalize. That syntax will still work, but the new syntax should be used for new development. (Read-Write) Set and query the state of Independent source normalization. Independent source must be ON (SOURce:ENABle) and in tracking mode SOurce:TRACking. |
|
Relevant Modes |
EMI, SA |
Parameters |
|
<bool> |
Normalization state. Choose from: ON (1) - Normalization ON OFF (0) - Normalization OFF |
Examples |
SOUR:NORM 1 |
Query Syntax |
SOURce:NORMalize? |
Return Type |
Boolean |
Default |
OFF |
Last Modified:
04no2022 |
Added EMI mode (12.3x) |
25-Mar-2014 |
Name change |
10-Oct-2010 |
New command (5.30) |