|
Note: This command was previously named SOURce:MODE. That syntax will still work, but this new syntax should be used for new development. (Read-Write) Set and query the source tracking. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<char> |
Source tracking type. Choose from: OFF - Disables tracking. TCF - Sets the internal source tracking to the center frequency. TPG - Sets the internal source tracking to the Pulse Generator. (Only available for model B/C and with option 357 Pulse Generator is licensed) TSWP - Sets the internal source to track with the SA receiver.(Only available for SA that has proper licensing for Tracking Generator capability) Use SOURce:NORMalize to normalize the trace. |
|
Examples |
SOUR:TRAC TCF |
|
Query Syntax |
SOURce:TRACking? |
|
Return Type |
Character |
|
Default |
OFF |
Last Modified:
|
04jul2024 |
Added new parameter TPG and SOUR:TRAC & SOUR:MODE's parameter equipvalency note (A.13.10) |
|
04nov2022 |
Added EMI mode (12.3x) |