SOURce:POWer:ATTenuation <num>

Note: This command was previously named [:SENSe]:ISOurce:POWer:ATTenuation. That syntax will still work, but the new syntax should be used for new development.

(Read-Write) Set and query the Independent Source attenuation level.

Use SOURce:ENABle to enable Independent Source.

Relevant Modes

SA  (N9912A ONLY - See SOURce:POWer:MAXimum and SOURce:POWer for all other models).

Parameters

 

<num>

Independent source attenuation in dB. Choose a value between 31 and 0.

This command will accept MIN and MAX as arguments.

Examples

SOUR:POW:ATT 20

source:power:att min

Query Syntax

SOURce:POWer:ATTenuation?

Return Type

Numeric

Default

10


Last Modified:

7-Apr-2014

Name change

10-Oct-2010

New command (5.30)