Note: This command was previously named [:SENSe]:ISOurce:POWer:MAXimum. That syntax will still work, but the new syntax should be used for new development. (Read-Write) Set and query the state of maximum Independent Source Power. Use SOURce:ENABle to enable Independent Source. |
|
Relevant Modes |
EMI, SA (All models EXCEPT N9912A - See SOURce:POWer:ATTenuation for this model). |
Parameters |
|
<bool> |
Max Independent Source Power state. Choose from: ON (or 1) - Independent Source Power level is set to the maximum achievable power at all frequencies. OFF (or 0) - Independent Source Power level is set using SOURce:POWer. |
Examples |
SOUR:POW:MAX 1 source:power:maximum off |
Query Syntax |
SOURce:POWer:MAXimum? |
Return Type |
Boolean |
Default |
OFF |
Last Modified:
04no2022 |
Added EMI mode (12.3x) |
25-Mar-2014 |
Name change |
10-Oct-2010 |
New command (6.00) |