SOURce:POWer <num>

Note: This command was previously named [:SENSe]:SOurce:POWer. That syntax will still work, but the new syntax should be used for new development.

(Read-Write) Set and query the Independent Source power level. This command automatically sets SOURce:POWer:MAXimum to OFF.

Use SOURce:ENABle to enable Independent Source.

Relevant Modes

 EMI, RTSA, SA  (All models EXCEPT N9912A - See [:SENSe]:ISOurce:POWer:ATTenuation for this model).

Parameters

 

<num>

Power level in dBm. Choose a value between -45 and 0.

This command will accept MIN and MAX as arguments.

Examples

SOUR:POW -20

source:power min

Query Syntax

SOURce:POWer?

Return Type

Numeric

Default

-15 dBm


Last Modified:

04no2022

Added EMI mode (12.3x)

25-Mar-2014

Name change

10-Oct-2010

New command (6.00)