SYSTem:ANTenna:EMF:AXIS <char>

(Read-Write) Set and query the EMF triaxial (USB) antenna axis.

NOTE: This command supersedes SYST:ANT:USB:AXIS. To learn  more, refer to Replacement Commands topic.

Relevant Modes

5G EVM, EMI, USB (EMF) Antenna, Pulse Generator

Couplings    

None

Parameters

 

<char>

AXIS value for manual control. Choose from:

AUTO – Manual axis control is disabled (off). All axes are selected and controlled by the instrument.

NOTE: Manual axis control was disabled by "N". This parameter is no longer valid.

X – X axis is selected for manual control.

Y – Y axis is selected for manual control.

Z – Z axis is selected for manual control.

Examples

SYST:ANT:EMF:AXIS X */Selects the X axis for manual control.

Query Syntax

SYST:ANT:EMF:AXIS?

Return Type

Character

Default

N (Manual axis control is off)


Last Modified:

06mar2024

Added new compatible command for EMF mode (A.13.00)