SYSTem:HEAD:CORRections[:STATe] <bool>

(Read-Write) Set and query frequency extender head corrections being shared from SA mode.

Relevant Modes

5G NR, 5G NR EVM Conducted, 5G TF, EMI, IQA, LTE FDD, PAA, RTSA, SA

Parameters

 

<char>

Choose from:

ON (1) - share frequency head corrections ON

OFF (0) - share frequency head corrections OFF

Examples

SYST:HEAD:CORR 1 */Enables the sharing of SA mode frequency extender head corrections

Query Syntax

SYSTem:HEAD:CORR?

Return Type

Boolean

Default

OFF (0)


Last modified:

04no2022

Added EMI mode (12.3x)

14apr2020

Added for A.12.00 FW (Compatible with OTA, PAA, RTSA, & SA Modes)