(Read-Write) Set and query the high sensitivity state when the frequency extender is enabled. |
|
Relevant Modes |
5G NR, 5G NR EVM Conducted, 5G TF, EMI, IQA, LTE FDD, PAA, RTSA, SA |
Parameters |
|
<char> |
Choose from: ON (1) - high sensitivity state ON OFF (0) - high sensitivity state OFF |
Examples |
SYST:HEAD:HIGH 0 */Disables the high sensitivity state |
Query Syntax |
SYSTem:HEAD:HIGH? |
Return Type |
Boolean |
Default |
OFF (0) |
Last modified:
04no2022 |
Added EMI mode (12.3x) |
14apr2020 |
Added for A.12.00 FW (Compatible with OTA, PAA, RTSA, & SA Modes) |