SYSTem:MAP:DISPlay:IMPort <string>


(Read-Write) Set and query the *.zip to be be unzipped in the destination folder.

See also, SYST:MAP:DISP:DEV[:DEST] and SYST:MAP:DISP:SOUR.

Relevant Modes

Channel Scanner, 5G NR, 5G TF, 5G NR EVM Conducted, LTE FDD, and PAA

Parameters

 

<"FileToUnzip">

Enter a zip filename to be unzipped. Use the following commands to set up the destination and source locations for your zip file: SYST:MAP:DISP:DEV[:DEST] and 

SYST:MAP:DISP:SOUR

 

Examples

SYST:MAP:DISP:IMP "ExampleFileToUnzip.zip"

Query Syntax

SYST:MAP:DISP:IMP?

Return Type

string

Default

n/a


Last Modified:

01dec2020

Updated command (12.1x)

09dec2019

Added new Mapping content (11.5x).