(Read-Write) Set and query the source of FieldFox trigger signals. |
|
Relevant Modes |
IQA, 5G NR, 5G NR EVM Conducted, 5GTF, SA, LTE FDD, PAA, RTSA |
Parameters |
|
<character> |
Trigger source. Choose from: Note: For PAA mode, the only applicable parameters are EXTernal and FREErun.
Note: Trigger Source selection does NOT have an impact on SA STEP sweeps. Trigger source is only implemented for Zerospan, IQ Captures, and FFT type sweeps. If a Trigger souce is selected when in STEP sweep the instrument displays the following popup message: FREE - (Free run) Triggering is provided by the FieldFox internal circuitry. A new sweep begins when the previous sweep ends. EXT - (External) A sweep is triggered on an external TTL signal at the External Trigger connector. VID - (Video) - (Not applicable for OTA (e.g., LTE FDD, LTE TDD, and 5GTF). Only available for SA, RTSA, and IQA.) - A sweep is triggered on a signal at the SA RF Input connector when the amplitude of the incoming signal exceeds the settable Trigger Level. RFB - (RF Burst) - (Not applicable for OTA (e.g., LTE FDD, LTE TDD, and 5GTF). Only available for SA, RTSA, and IQA.) - Similar to Video triggering, a sweep is triggered from a signal at the SA RF Input connector. However, an RF Burst trigger is detected in the third IF stage. A sweep is triggered when the amplitude of the incoming signal exceeds the settable Trigger Level. Note: Learn more about RF Burst in the N9927-90020 User's Guide and N9938-90006 User's Guide. FRAMe (Periodic) - Trigger repeats at the period rate entered. Periodic trigger’s phase can be altered by the Offset value. See AlsoTRIGger[:SEQuence]:VIDeo:LEVel (SA Only) TRIGger[:SEQuence]:VIDeo|RFBurst:LEVel (IQA Only)
|
Examples |
TRIG:SOUR EXT |
Query Syntax |
TRIGger[:SEQuence]:SOURce? |
Return Type |
Character |
Default |
FREE |
Last Modified:
25apr2022 |
Updated descriptions (12.4x) |
10dec2019 |
Added 5G NR, PAA, and 5G NR EVM Conducted (11.5x) |
28nov2018 |
Added LTE FDD & 5GTF (11.0) |
22-Oct-2017 |
Added IQA mode (10.1x) |
10-june-2016 |
Added RTSA mode (9.50) |
28-Mar-2013 |
Added RF Burst (6.25) |