Start the PLTS Software


Other Getting Started Topics

Start the PLTS software by doing either of the following:

Keysight PLTS Connection Manager Server

Every time you start PLTS, the Keysight PLTS Connection Manager Server verifies that essential components of the PLTS installation are working.

Identify the License and Start PLTS Software

Note:

Beginning with PLTS release 3.12, a floating license can now be installed on Solaris and HP-UX servers.

For a complete description of the licensing process, refer to Chapter 3 of the PLTS Installation Manual.

Important PLTS License Note:

From July 1, 2020, PLTS2020 update 1 release (PLTS2020U1), we implemented Keysight Advanced License (KAL). For PLTS orders after July 1, 2020, PLTS uses the KAL license.

For the KAL license, users need to use Keysight PathWave License Manager to add and manage the licenses.

PLTS software will automatically install "Keysight PathWave License Manager" to your PC.

Before the first start of the PLTS software, we recommend you add KAL license in "Keysight PathWave License Manager."

Procedure to add Keysight Advanced Licensing (KAL)

NOTE: PathWave License Manager has been renamed to Keysight Software Manager Utility (KSM-U). KSM-U is the preferred method for installing and managing licenses for PLTS software. Learn more and download KSM-U at keysight.com/find/KSMU.

  1. Open ”Keysight PathWave License Manager” in your Windows start menu to add your KAL licenses: :


  2. To add a license to the PC, click on the Add a License File button, choose the license file to add, then click on the Add Now button.

If you didn't add the license before the first start of PLTS

If you didn’t add the license before the first start of PLTS, when PLTS starts and can’t find a qualified license, PLTS will display a dialog with instructions. Follow the steps in the dialog to add the licenses or run in free viewer mode without a license:

Note:  Make a back-up copy of the license file if you have not already done so.

Find Hardware

It would be very time-consuming for PLTS to look for hardware at every GPIB interface and address each time PLTS is started. This is especially true considering that most people use the same hardware every time. The following is the process that PLTS uses to establish and communicate with your PLTS hardware:

When PLTS is started, it looks for the same system at the same addresses that were used that last time PLTS was run.

PLTS Rescan looks for instruments using the Keysight IO Library's list of instruments / addresses.

Note: Problems finding instruments when using Keysight IO Libraries Version Suite 14.

If there were instruments on the bus and then removed or turned off, they stay in the Keysight IO Libraries list of instruments. When PLTS rescans for instruments, they are not found and timeout messages are displayed for the missing instruments. It is necessary to manually delete the instruments from the configuration in the Keysight IO Library Connection Expert.

 

Build Logical Measurement System

If PLTS finds more than one system on the GPIB, it displays the Build Logical Measurement System dialog box. This dialog box allows you to identify your PLTS system hardware for the PLTS software. To identify your system:

  1. In the Instruments Found list, click the model number of your VNA or TDR instrument. Then click Primary Inst >>  which moves the model number to the text box at the right of the button.

  2. If using a VNA test set, in the Instruments Found list, click the model number of your test set. Then click Secondary Inst >> which moves the model number to the text box at the right of that button.

  3. Click Create System which moves the combination of the devices to the Logical Measurement System box.

  4. Click OK to save the system so the software identifies the PLTS system.

Manual Configuration

If your system does not identify hardware automatically, you can manually configure your system by selecting the Manual Configuration button to display the Hardware Configuration dialog box. This procedure was necessary with older PLTS test sets.

  1. Select the primary instrument (typically at VNA or a TDR) from the Primary Instrument list. If necessary, select a secondary instrument (typically at test set) from the Secondary Instrument list.

  2. Enter the address for the primary instrument in the Analyzer Address text box and the secondary instrument in the Test Set Address text box. Also, enter the VISA Interface Name.

Select (Virtual) Measurement System

If PLTS does NOT recognize a PLTS system, it notifies you: “No instruments were detected. PLTS will operate in analysis-only mode.” Select the virtual instrument that best matches your PLTS system or if known, the system that was used to measure data that you will be loading for analysis.

Note: The selection highlighted above is a PNA-L with a 12-port test set.

For more information about making measurements see either:

Scan for New Hardware

Click Tools, then Acquisition Hardware, then either Choose Data Acquisition Device or Scan (or Re-scan) for New Hardware.