Wideband Pulsed Application


Note: The PNA-X with Opt 025 and Opt 008 has an integrated Pulse Measurement Setup that makes this application no longer necessary on the PNA-X.

The Wideband Pulsed Application configures the PNA-X internal pulse generators and modulators for measuring pulsed S-parameters using the wideband mode detection technique.

The Wideband Pulse Application is designed to be used with the PNA-X with Opts 021, 022, and 025.

Note: Wideband Pulse application is NOT supported on the E836x and PNA-L models.

See Also

Download and Install the Wideband Pulsed Application

This application is installed and run as a macro on the PNA-X. Learn more about macros.

  1. Go to http://na.support.keysight.com/pna/apps/applications.htm

  2. Click the download link

  3. Save the downloaded file to the PNA hard drive

  4. Double-click the downloaded file to install the Wideband Pulsed Application on the PNA.

  5. The application is saved on the PNA at C:/Program Files/Keysight/Network Analyzer/Applications/WB Pulse/Wideband_pulse.exe

  6. Configure the macro. Learn how.  

To learn more about Wideband pulsed application, click Help in the application.