Write-only
About Markers

InterpolateMarkers Method


Description

Turns All Marker Interpolation ON and OFF for the measurement. Marker interpolation enables X-axis resolution between the discrete data values. The analyzer will calculate the x and y-axis data values between discrete data points. To override this property for individual markers, use the Interpolated property.

 VB Syntax

meas.Interpolate = value

Variable

(Type) - Description

meas

A Measurement (object)

value

(boolean)
False
- Turns interpolation OFF for all markers in the measurement
True
- Turns interpolation ON for all markers in the measurement

Return Type

Boolean

Default

True (ON)

Examples

meas.Interpolate = 1

C++ Syntax

HRESULT InterpolateMarkers(VARIANT_BOOL bNewVal)

 Interface

IMeasurement