Write/Read
About Markers

Interpolated Property


Description

Turns marker Interpolation ON and OFF. Marker interpolation enables X-axis resolution beyond the discrete data values. The analyzer will calculate the x and y-axis data values between discrete data points. Use meas.Interpolate to change interpolation of all markers in a measurement. This command will override the measurement setting.

 VB Syntax

mark.Interpolated = value

Variable

(Type) - Description

mark

A Marker (object)

value

(boolean)
False
- Turns interpolation OFF

True - Turns interpolation ON

Return Type

Boolean

Default

True

Examples

mark.Interpolated = True 'Write

interpolate = mark.Interpolated 'Read

C++ Syntax

HRESULT get_Interpolated(VARIANT_BOOL *pVal)
HRESULT put_Interpolated(VARIANT_BOOL newVal)

Interface

IMarker