Write-only
About Dynamic Uncertainty

Save Method


Description

Saves an uncertainty ‘workspace’ (*.ml4) file from the Uncertainty Manager.

VB Syntax

uncertMan.Save (fileName)

Variable

(Type) - Description

uncertMan

An UncertaintyManager Object

fileName

(String). Filename and *.ml4 extension of the Uncertainty Manager workspace file to save.

If filename is omitted or NULL (0) is passed for this argument, then Uncertainty Manager’s current workspace is saved to whichever filename that current workspace had been recalled from, even if changes had been made to the workspace since that last Recall.

Return Type

Not Applicable

Default

Not Applicable

Examples

uncertMan.Save "MyWorkspace.ml4" 'saves to the specified workspace filename.

uncertMan.Save 'saves to the current workspace filename.

See example program

C++ Syntax

HRESULT Save([in, defaultvalue(0)] BSTR fileName);

Interface

IUncertaintyManager