Write-only
About PNOP Marker Search

SearchPowerNormalOperatingPoint Method


Description

Initiates a PNOP marker search.

Turns on and sets markers 1, 2, 3, and 4 to calculate various PNOP parameters.

First set BackOff and PinOffset.

To turn off these markers, either turn them off individually or DeleteAllMarkers.

To search a UserRange, first activate marker 1 and set the desired UserRange. Then send the SearchPowerNormalOperatingPoint command. The user range applies only to marker 1 searching for the max value. The other markers may fall outside the user range.

 VB Syntax

pnop.SearchPowerNormalOperatingPoint( )

Variable

(Type) - Description

pnop

A PNOP (object)

Return Type

Not Applicable

Default

Not Applicable

Examples

pnop.SearchPowerNormalOperatingPoint

See example program

C++ Syntax

HRESULT SearchPowerNormalOperatingPoint()

Interface

IPNOP