Write-only
About Spectrum Analyzer Markers

toSA Method


Description

Creates an SA channel with a marker at the same CW frequency. Learn more.

 VB Syntax

mkr.toSA

Variable

(Type) - Description

mkr

A Marker (object)

Return Type

Not Applicable

Default

Not Applicable

Examples

See example program

C++ Syntax

HRESULT toSA( )

Interface

IMarker6