Controls the noise figure calibration settings for amplifiers and converters. These commands supplement the standard calibration commands on the GuidedCalibration Object.
|
Dim app as AgilentPNA835x.Application Set noisecal = pna.GetCalmanager.CreateCustomCalEx(channelNum) Set noiseCalExtension = noisecal.CustomCalConfiguration noiseCalExtension.NoiseSourceCold = 300 |
Examples:
Method |
InterfaceSee History |
Description |
|---|---|---|
|
None |
|
|
Property |
Interface |
Description |
|
INoiseCal2 |
Sets the state of auto orientation for a noise tuner during Noise Figure for NFX. |
|
|
INoiseCal |
Sets and returns the method for performing calibration on a noise channel. |
|
|
INoiseCal2 |
Enables and disables LO power calibration for NFX. |
|
|
INoiseCal |
Sets and returns the name of the ENR file associated with the noise source. |
|
|
INoiseCal2 |
Sets and reads the state of ENR adapter de-embedding. |
|
|
INoiseCal2 |
Sets and reads the state of noise source adapter de-embedding. |
|
|
INoiseCal |
Sets and reads the Cal Kit type used to perform a cal at the adapter which is used to connect the noise source (if required.) |
|
|
INoiseCal |
Sets and returns the current temperature at the noise source. |
|
|
INoiseCal |
Sets and reads the connector type of the noise source used during the cal. |
|
|
INoiseCal3 |
Set and read the method used to characterize the noise receivers. |
|
Interface |
Introduced with PNA Rev: |
|
INoiseCal |
8.0 |
|
INoiseCal2 |
9.10 |
|
INoiseCal3 |
9.70 |
Last Modified:
|
9-Jun-2011 |
Added INoise3 |
|
30-May-2007 |
MX New topic |