Write/Read
About Noise CAL

AutoOrientTunerTuner Property


Description

Sets the state of auto orientation for a noise tuner during Noise Figure for NFX.

 VB Syntax

nfCal.AutoOrientTuner = bool

Variable

(Type) - Description

nfCal

A NoiseCal (object)

bool

(Boolean)

True - Set AutoOrientTuneration ON

False - Set AutoOrientTuneration OFF

Return Type

Boolean

Default

True

Examples

nfCal.AutoOrientTuner = True

C++ Syntax

HRESULT put_AutoOrientTuner(VARIANT_BOOL bEnable);

HRESULT get_AutoOrientTuner(VARIANT_BOOL *bEnable);

Interface

INoiseCal2