Write/Read
About SA Application

EnableADCFilterAuto Property


Description

Set and read how the ADC filter is set. When set to 1, ADC filter is set based on the ADC sampling frequency.

VB Syntax

sa.EnableADCFilterAuto = value

Variable

(Type) - Description

sa

A SpectrumAnalyzer (object)

value

(Boolean) Choose from:

0 - OFF - ADC filter is set manually using ADCFilter.

1 - ON - Automatically select ADC filter based on the ADC sampling frequency.

Learn about these settings.

Return Type

Boolean

Default

1

Examples

sa.EnableADCFilterAuto = 0  'Write

value = sa.EnableADCFilterAuto 'Read

See an example program.

C++ Syntax

HRESULT put_EnableADCFilterAuto(VARIANT_BOOL bEnable);

HRESULT get_EnableADCFilterAuto(VARIANT_BOOL* bEnable);

Interface

ISpectrumAnalyzer