Write/Read |
About SA Application |
Description |
Set and read how the ADC sample rate is set. When set to 1, ADC sample rate is set based on the ADC filter setting. |
VB Syntax |
sa.EnableADCSampleRateAuto = value |
Variable |
(Type) - Description |
|
sa |
A SpectrumAnalyzer (object) |
|
value |
(Boolean) Choose from: 0 - OFF - ADC sampling rate is set manually using ADCSampleRate. 1 - ON - Automatically select ADC sample rate based on the ADC filter setting. |
Return Type |
Boolean |
Default |
1 |
Examples |
sa.ADCSampleRateAuto = 1 'Write |
|
value = sa.ADCSampleRateAuto 'Read |
|
C++ Syntax |
HRESULT put_ADCSampleRateAuto(VARIANT_BOOL bEnable); HRESULT get_ADCSampleRateAuto(VARIANT_BOOL* bEnable); |
Interface |
ISpectrumAnalyzer |