Write/Read
About Active Match

AbsoluteExtractionToneLevel Property


Description

Set and read the absolute tone power level.

 VB Syntax

HotS22.AbsoluteExtractionToneLevel = level

Variable

(Type) - Description

HotS22

A ActiveParametersApp (object)

level

(Double) - Absolute tone power level

Return Type

Double

Default

-5 dBm

Examples

HotS22.AbsoluteExtractionToneLevel = -5 'Write

level = HotS22.AbsoluteExtractionToneLevel 'Read

C++ Syntax

HRESULT get_AbsoluteExtractionToneLevel(double* level)

HRESULT put_AbsoluteExtractionToneLevel(double level)

Interface

IActiveChannelSettings