Write/Read |
About Diff I/Q App |
Description |
Sets and reads the ON/ OFF state of auto range source attenuation. On the Source Configuration dialog under Power, this is the Auto range source attenuator setting. |
VB Syntax |
DIQ.AutoRangeState (port) = value |
Variable |
(Type) - Description |
|
DIQ |
A Differential I/Q (object) |
|
port |
(String) Source port name. Use SourcePortNames to read a list of valid source ports. |
|
value |
(Boolean) Choose from:
|
Return Type |
Boolean |
Default |
ON |
Examples |
diq.AutoRangeState = True 'Write |
|
value = diq.AutoRangeState 'Read |
|
C++ Syntax |
HRESULT get_AutoRangeState(BSTR port, BOOL* AutoRangeState); HRESULT put_AutoRangeState(BSTR port, BOOL AutoRangeState); |
Interface |
IDifferentialIQ |
Last modified:
|
18-Mar-2014 |
New topic |