Write/Read
About Spectrum Analyzer Markers

BandpowerSpan Property


Description

Sets and reads the frequency span of  the band power marker. This area is marked by two vertical dotted lines on the screen and the marker's y-axis value is set to the measured power value. Noise and power on the same marker share the same span.

VB Syntax

mkr.BandpowerSpan = value

Variable

(Type) - Description

mkr

A Marker (object)

value

(Double) Choose a frequency span within the frequency range of the analyzer.

Return Type

Double

Default

1 MHz

Examples

See example program

C++ Syntax

HRESULT get_BandpowerSpan(double* pVal)

HRESULT put_BandpowerSpan(double newVal)

Interface

IMarker6