Write/Read
About SA Application

BandwidthNarrowMax Property


Description

Set and read the maximum value for narrow DFT bandwidth. The maximum narrow DFT bandwidth setting is 11 MHz. The AutoBandwidth must be set to OFF to set this value manually.

VB Syntax

sa.dft.BandwidthNarrowMax = value

Variable

(Type) - Description

sa.dft

A SpectrumAnalyzerDFT (object)

Return Type

Double

Examples

sa.dft.BandwidthNarrowMax = 11e6  'Write

value = sa.dft.BandwidthNarrowMax 'Read

C++ Syntax

HRESULT put_BandwidthNarrowMax(double maxbw);

HRESULT get_BandwidthNarrowMax(double* maxbw);

Interface

ISpectrumAnalyzerDFT