Write/Read |
About Performing a Calibration |
Description |
Note: This command has been replaced by CalibrationTypeID_property, which provides selection of Calibration Type by string. Specifies the type of calibration to perform or apply to the active S-Parameter measurement. This command determine the ports involved in the CalType by the ports being used by the active measurement. For example:
Note: For FCA measurements, use CalibrationName and CalibrationTypeID. |
VB Syntax |
meas.CalibrationType = type |
Variable |
(Type) - Description |
meas |
A Measurement (object) |
type |
(enum NACalType) - Calibration type. Choose from: 0 - naCalType_Response_Open 1 - naCalType_Response_Short 2 - naCalType_Response_Thru 3 - naCalType_Response_Thru_And_Isol 4 - naCalType_OnePort 5 - naCalType_TwoPort_SOLT 6 - naCalType_TwoPort_TRL 7 - naCalType_None 8 - naCalType_ThreePort_SOLT 9 - Custom 10 - naCalType_FourPort_SOLT |
Return Type |
NACalType |
Default |
naCalType_None |
Examples |
meas.CalibrationType = naCalType_Response_Open 'Write |
meascal = meas.CalibrationType 'Read |
|
C++ Syntax |
HRESULT put_CalibrationType (tagNACalType CalType) |
Interface |
IMeasurement |