The following calibration types are available in the PNA.
|
Cal Type |
Interface |
Accuracy |
Thru Methods allowed |
|
Both |
Very High |
All except Unknown Thru |
|
|
Both |
High |
All |
|
|
SmartCal |
High |
Defined Thru or Flush Thru |
|
|
QSOLT (Quick SOLT) |
SmartCal |
Medium |
Defined Thru or Flush Thru |
|
Both |
High |
Not Applicable |
|
|
Open/Short Response |
Unguided |
Low |
Not Applicable |
|
Thru Response |
Unguided |
Low |
Known Thru or Flush Thru |
Learn how to select a default Cal Type.
Application: Used to accurately calibrate any pair of ports when calibration standards are not readily available.Note: A Delta Match Cal may be required. • Learn more about TRL family cal • For more information on modifying standards, see Calibration Standards. |
Calibration Method: SmartCal, Unguided Calibration |
General Accuracy: Very High |
Standards Required: THRU, REFLECT, LINE or similar combination |
Systematic Errors Corrected:• Directivity• Source match• Isolation (see exceptions)• Load match• Frequency response transmission tracking• Frequency response reflection tracking |
Application: Used to accurately calibrate any number of ports. |
General Accuracy: High |
Calibration Method: SmartCal, Unguided Calibration, ECal |
Standards Required: (SHORT, OPEN, LOAD, THRU) or ECal module |
Systematic Errors Corrected (on all ports):• Directivity• Source match• Isolation (see exceptions)• Load match• Frequency response transmission tracking• Frequency response reflection tracking |
Application: Used to calibrate two ports when only measurements in one direction (forward OR reverse) are required. Measurements are faster because a second sweep is NOT required.• Reflection Standards (OPEN, SHORT, LOAD) are connected to the source port to be calibrated.• Defined THRU or Flush THRU standard is connected between port pairs. • Much quicker than SOLT when using a mechanical cal kit. ECal can also be used.To select Enhanced Response: For a standard S-parameter Cal, select SmartCal in the Cal Wizard. Then, for all cals:
Enhanced Response cal also be selected as the default Cal Type using Cal Preferences. |
General Accuracy: High |
Calibration Method: SmartCal, ECal |
Standards Required: (SHORT, OPEN, LOAD, Defined THRU or Flush THRU) |
Systematic Errors Corrected:• Directivity (source port)• Source match (source port)• Isolation (see exceptions)• Load match (receiver port) - used only to produce transmission tracking term.• Frequency response transmission tracking (receiver port).• Frequency response reflection tracking (source port). |
Application: Used to quickly calibrate any number of ports. Developed specifically for use with external multiport test sets.Note: A Delta Match Cal is required to cal test ports that do not have a dedicated reference receiver. • Reflection Standards (OPEN, SHORT, LOAD) are connected to only ONE of the ports to be calibrated. The lower port number of the ports to be calibrated is selected by default. This can be changed through the Modify Cal / Cal Type setting.• Defined THRU or Flush THRU standards are connected from the reflection standard port to the remaining ports to be calibrated. • Much quicker than SOLT when using a mechanical cal kit.• Based on TRL math. |
General Accuracy: Not as high as SOLT |
Calibration Method: SmartCal, ECal |
Standards Required: (SHORT, OPEN, LOAD, Defined THRU or Flush THRU) |
Systematic Errors Corrected:• Directivity• Source match• Isolation (see exceptions)• Load match• Frequency response transmission tracking• Frequency response reflection tracking |
Application: Used to accurately calibrate any single test port for reflection measurements only. |
Calibration Method: SmartCal, Unguided Calibration, ECal |
General Accuracy: High |
Standards Required: (SHORT, OPEN, LOAD) or ECal module |
Systematic Errors Corrected:• Directivity• Source match• Frequency response reflection tracking |
Application: Used to quickly calibrate any single test port for reflection measurements only. |
Calibration Method: Unguided Calibration |
General Accuracy: Low |
Standards Required: OPEN or SHORT |
Systematic Errors Corrected:Frequency response reflection tracking |
Application: Used to quickly calibrate any pair of test ports for transmission measurements only.Isolation is not usually recommended. Learn more about Isolation |
Calibration Method: Unguided Calibration and Guided Cal from the 'Select DUT Connectors page', check Modify Cal, then click Next. |
General Accuracy: Low |
Standards Required: THRUIsolation: One LOAD for each PNA test port. |
Systematic Errors Corrected:• Frequency response transmission tracking• Isolation |
Last modified:
|
24-May-2013 |
Edit transmission resp |
|
5-Sep-2008 |
Added note for ER Load Match |
|
16-Apr-2008 |
Removed AR for TRL limitation |
|
23-Feb-2007 |
Added Enhanced Response |
|
12-Sept-2006 |
Added QSOLT |