Write / Read | 
About Frequency Settings | 
Description | 
 Sets and reads how the center frequency step size is determined. When TRUE, center steps by 5% of span. When FALSE, center steps by STEP:SIZE value.  | 
VB Syntax | 
 chan.CenterFrequencyStepSizeMode = value  | 
Variable | 
(Type) - Description | 
| 
 chan  | 
 (object) - A Channel object  | 
| 
 value  | 
 (Enum as NAModes) Choose from: 0 - naAUTO -Step size is set automatically. 1 - naMaunal - Step size is set manually using CenterFrequencyStepSize Property.  | 
Return Type | 
 Enum  | 
Default | 
 1 - naMaunal  | 
Examples | 
 chan.CenterFrequencyStepSizeMode = naAUTO 'Write value = chan.CenterFrequencyStepSizeMode 'Read  | 
C++ Syntax | 
 HRESULT get_CenterFrequencyStepSizeMode(tagNAModes* pVal); HRESULT put_CenterFrequencyStepSizeMode(tagNAModes pVal);  | 
Interface | 
 IChannel25  |